ON Semiconductor Expands Serial EEPROM Portfolio

Introduction Includes New High Density Devices for the Automotive, Medical, and Consumer Markets

EEPROM Memory CAT24M01 image

PHOENIX, Ariz. – June 22, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance silicon solutions for energy efficient electronics, has released new EEPROM (Electrically Erasable Programmable Read-Only Memory) devices for the automotive, medical, and consumer markets.

The EEPROM devices include the high density 512 kilobit (kb) CAT24C512 and 1 megabit (Mb) CAT24M01, which have a 1.8 volt (V) to 5.5 V supply voltage range. The CAT24C512 and CAT24M01 employ 256 byte and 128 byte page write buffers respectively. Both devices support Standard 100 kilohertz (kHz), Fast 400 kHz, and Fast-Plus 1 megahertz (MHz) serial I2C protocols. These devices are manufactured on a 0.18 micrometer (µm) low power CMOS process at the ON Semiconductor owned and operated Gresham, Oregon facility.

In addition, the company introduced a series of AEC-Q100 qualified EEPROMs for automotive designs. These devices have a 2.5 V to 5.5 V supply voltage range and support the Standard and Fast I2C protocols. Both the 64 kb CAV24C64 and the 32 kb CAV24C32 feature 32 byte page write buffers, while the 2 kb CAV24C02, 4 kb CAV24C04, 8 kb CAV24C08 and 16 kb CAV24C16 incorporate a 16 byte page write buffer.  These devices are also manufactured at the Gresham facility, on a 0.35 µm process.

All of the new EEPROM devices feature a 100 year data retention period and support for 1,000,000 program/erase cycles.  The operating temperature range of these serial EEPROMs is −40 ⁰C to +125 ⁰C.

Further products will be added to the portfolio later this year, including versions of both the high density and automotive devices with SPI interfaces, to complement the I2C interface products.

 “The state-of-the-art ON Semiconductor facility in Gresham, Oregon, provides us with advanced, in-house manufacturing technology and substantial capacity to provide a stable supply chain for EEPROM products,” said Dev Nair, marketing director for EEPROM products at ON Semiconductor.  “We are pleased to be able to offer high density and automotive qualified I2C EEPROMs to our broad customer base, and look forward to expanding the portfolio further with SPI EEPROMs later this year.”

Packages and Pricing

The CAT24C512 and CAT24M01 are available in Pb-free, RoHS compliant SOIC-8, TSSOP-8 and PDIP-8 packages, and are priced at $0.90 per unit for CAT24C512 and at $1.50 per unit for CAT24M01 in quantities of 10,000 units.  The CAV24C02, CAV24C04, CAV24C08, CAV24C16, CAV24C32 and CAV24C64 are available in Pb-free, RoHS compliant TSSOP-8 and SOIC-8 packages, and are priced between $0.27 and $0.67 per unit.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.