New LGA-Packaged MOSFETs Help Maximize Efficiency and Battery Life in Space Limited Smart Phone and Tablet PC Applications

June 04, 2013

Single and dual Li-ion battery charging / discharging protection circuits benefit from high-performance FlipChip MOSFETs















New LGA-Packaged MOSFETs Help Maximize Efficiency

PHOENIX, Ariz. – June 4, 2013 – – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency,has introduced two new MOSFET devices designed for use in smart phone and tablet PC applications where they provide a crucial part of the Lithium ion (Li-ion) battery charging / discharging protection circuit switching. The EFC6601R Power MOSFET and EFC6602R Power MOSFET help designers to reduce solution size, improve efficiency and maximize battery life.

Suitable for single or dual Li-ion cell implementations, the new RoHS compliant devices offer industry-leading levels of RDS (on) performance and employ a Land Grid Array (LGA) structure to give them a small, low-profile design that makes them ideal for the limited space environment typical of smart phone and tablet PC applications. The EFC6601R has a specified maximum VSSS (Source to Source Voltage) of 24 volt (V), and the EFC6602R has a specified maximum VSSS of 12 V. Both devices operate from a 2.5 V supply, have a common-drain structure, and a built-in protection diode.

“Since the introduction of lithium ion batteries ON Semiconductor has been developing and supplying charging/discharging protection circuit switching MOSFETs,” said Takashi Akiba, general manager of MOS products for ON Semiconductor’s SANYO Semiconductor Products Group. “Our accumulated knowledge and expertise has enabled us to create these highly miniaturized devices that further help extend the battery life and enhance efficiency.”

ON Semiconductor plans to add five further devices to the EFC MOSFET family within the year that will help designers of an even wider range of mobile devices achieve their application objectives for reducing solution size and extending battery life.


Packaging and Pricing
The EFC6601R and EFC6602R are offered in halogen-free EFCP packages and are $0.80 and $1.00 in 5,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.