onsemi Unveils New High Power Totem Pole PFC Controller Meeting Challenging Efficiency Standard

Latest device reduces development time and cost allowing solutions to be delivered to market faster

PHOENIX – March 21, 2022 – onsemi (Nasdaq: ON), a leader in intelligent power and sensing technologies, introduced its latest mixed-signal controller dedicated to bridgeless totem pole PFC (TP PFC) topology. The NCP1681 targets ultra-high density offline power supplies. Building upon the success of theNCP1680, which is suited for designs up to 350 W, the new controller extends the power capability into the kilowatt range.

In the past, TP PFC designs required the use of an MCU that added design complexity and the need for coding. However, with the NCP1681, only a few external components and no coding is needed to be added for a fully-featured TP PFC solution, thereby saving time, cost and space.

Commenting on the new release, Robert Tong, Senior Vice President & General Manager of Computing and Cloud Division at onsemi said “The new NCP1681 extends the benefits of code-free TP PFC design into higher power. This allows our customers to continue to enhance the efficiency of their design while reducing design time and cost, thereby delivering solutions to market quickly.”

The NCP1681 can be configured to work in either fixed frequency continuous conduction mode (CCM) or multi-mode operation, where the controller naturally transitions between CCM and critical conduction mode (CrM) for optimal performance across power levels.

The new NCP1681 high power TP PFC controller integrates established control algorithms with novel features to deliver a high performance and cost-effective TP PFC solution. Challenging efficiency standards such as ‘80Plus’ or ‘CoC Tier 2’, that require high efficiency over a wide load range, can also be met.

The new NCP1681 is suited to higher-power power supplies from 350 W to several kilowatts range that operate on universal mains input (90 – 265 Vac), addressing a wide range of applications including server, high performance computing, telecom, industrial and OLED TV. At high line, NCP1681 TP PFC solutions will achieve close to 99% efficiency.

The NCP1681 will be demonstrated alongside the award-winning lower power (<300 W) NCP1680 at APEC 2022 , at the George R. Brown Convention Center in Houston, TX. The demonstrations can be found at onsemi’s booth (1124) from March 21 to March 23.

Alongside the TP PFC controllers, onsemi offers a wide range of SiC MOSFETs and isolated gate drivers that can be used for the fast leg of the totem pole. SiC MOSFET devices have low on resistance (RDS(on)) and compact chip size which ensures low capacitance and gate charge (Qg), delivering highest efficiency in a reduced system size, thereby enabling power density. When NCP1681 is used with NCP51561 galvanically isolated gate driver, robust design can be realized without sacrificing switching performance.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy