ON Semiconductor Supports International Power Supply Design Contest Sponsored by EPA and California Energy Commission

Share

Phoenix-based company lends its support to university design teams via technical assistance, complimentary semiconductor device kits and prize money to top three finishers

Applied Power Electronics Conference (APEC) – Anaheim, Calif. – Feb. 23, 2004 – To further encourage electrical engineering students worldwide to enter Efficiency Challenge 2004, an international power supply design contest being sponsored by the U.S. Environmental Protection Agency (EPA) and the California Energy Commission (Energy Commission), ON Semiconductor (Nasdaq: ONNN) today announced plans to extend its support to university design teams via technical assistance and complimentary semiconductor device kits. Additionally, ON Semiconductor will award monetary prizes to the top three finishers among the assisted universities in the entire competition.

Efficiency Challenge 2004 is endorsed by the Power Sources Manufacturers Association (PSMA) and is aimed at fostering the development and market success of energy efficient power supply designs. Two major design categories are being featured, according to an announcement released by the EPA and the Energy Commission. The first category will cover internal and external “market-ready” designs that can cost-effectively save energy in particular types of consumer electronics. The second is an “open” category intended to showcase the most effective power supply designs from industry and academia without cost constraints.

Powering Efficiency
It is estimated that between 1 and 2 percent of all the electricity currently used in the U.S. could be saved by efficiency improvements to power supply devices that convert ac power from wall outlets into low voltage dc power. This applies to the power conversion circuitry within electronic products such as cordless phones, computers, television sets, stereo equipment, cell phone chargers, and PDA docking stations.

Research funded by the EPA’s ENERGY STAR® program and the Energy Commission’s Public Interest Energy Research (PIER) program has identified ac-dc power supplies as a major opportunity for reducing global energy consumption and greenhouse gas emissions. Today, there are more than 3.1 billion power supplies in use in the U.S. and about 10 billion globally. Many of the power supply designs used in today’s consumer electronics are only 30 percent to 60 percent efficient – though technologies exist to achieve operating efficiencies of 90 percent.

While the international design competition will showcase highly efficient technologies, it is also focused on highlighting the benefits of advanced power supplies to electronics buyers. Opportunities to improve power efficiency and conserve electricity are available to companies that manufacture power supplies as well as much larger companies that purchase power supplies for use in computers, televisions, printers, monitors and more.

Efficiency Challenge 2004 will run throughout the 2004 calendar year, with the winners announced at APEC 2005. For more information, visit www.efficientpowersupplies.org.

University Participation
ON Semiconductor will assist up to a total of 10 universities – domestically and internationally - that apply to participate in this competition. Applications for this assistance must be submitted by April 15, 2004. ON Semiconductor’s assistance will consist of the following:
• ON Semiconductor evaluation board(s) provided at no charge
• Engineering assistance from the company’s engineering experts (field application engineers or systems engineers)
• Relevant samples available from the company’s entire device portfolio
• Dedicated email support line
• Access to regional labs for testing (limited to 8 hours).

For application information, visit www.onsemi.com/power or contact Dhaval Dalal at 602.244.3759.

About ON Semiconductor
ON Semiconductor (Nasdaq: ONNN) offers an extensive portfolio of power- and data-management semiconductors and standard semiconductor components that address the design needs of today’s sophisticated electronic products, appliances and automobiles. For more information visit ON Semiconductor’s web site at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its web site in this news release, such information on the web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.