ON Semiconductor’s New Integrated LED Driver Improves System Efficiency for Low Bay, Street and Architectural Lighting Applications

PHOENIX, Ariz. – July 7, 2010 –

Share

NCL30001 features power factor correction and step-down power conversion in a single stage which helps reduce overall part count and system costs

PHOENIX, Ariz. – July 7, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics today announced the further expansion of its solutions for LED lighting with the introduction of an offline LED driver that integrates power factor correction (PFC) and isolated step-down AC-DC power conversion in a single stage. By eliminating the need for a dedicated PFC boost stage, the NCL30001 offers a reduced component count, lower cost solution that supports higher overall system efficiency in LED power supplies for applications such as LED-based street, low bay, wall packs, and architectural lighting.

Ideal for designs with power requirements of between 40 W and 150 W, the NCL30001 is designed to operate in continuous conduction mode (CCM) and can be configured as either a constant current or fixed output voltage driver. With an adjustable operating frequency of 20 kHz to 250 kHz and a multi-function latch-off pin able to implement an overtemperature shutdown circuit, the SOIC-16 packaged controller offers circuit designers a high degree of flexibility.

Further features of the NCL30001 controller’s specification include a high voltage start-up circuit, voltage feedforward to improve loop response, a brownout detector, internal overload timer, latch input and a high accuracy multiplier to reduce input line harmonics. An isolated single stage power factor corrected LED Driver evaluation board is available for this device that is intended for applications ranging from 40 W – 100 W that require a direct constant current output, The current is adjustable from 0.7 A to 1.5 A. to support a wider range of high power high brightness LEDs.

“With growth in the popularity and the rapidly increasing number of LED-based lighting designs on the market, the need for highly efficient, cost effective, integrated system management devices is greater than ever,” said Christophe Warin, AC-DC Business Unit Manager, ON Semiconductor. “The NCL30001 meets these requirements in full, and provides engineers with a flexible single-stage topology LED driver ideal for use in their new LED lighting products. This device is a strong example of the targeted lighting solutions ON Semiconductor is developing to meet our customers’ needs.”

The NCL30001 is available in a 16-lead SOIC package and priced at $1.05 per unit in 10,000 unit quantities.

For more information, please visit www.onsemi.com.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.