ON Semiconductor Introduces Industry Leading, Best in Class System Level Performance Expansion to IGBT Portfolio

May 14, 2013

New IGBT devices expand current ratings and deliver efficient, high-speed switching capabilities for power applications such as UPS, hot pots, rice cookers and microwave appliances















New generation Field Stop II (FSII) devices improve switching characteristics and reduce losses by up to 30 percent

Power Conversion Intelligent Motion (PCIM), NUREMBERG, Germany – May 14, 2013 – – ON Semiconductor (Nasdaq: ONNN),driving innovation in energy efficiency, continues to expand its portfolio of high performance IGBTs targeted at high performance power conversion (HPPC) consumer appliance and industrial applications. The new generation Field Stop II (FSII) devices being launched at PCIM improve switching characteristics and reduce losses by up to 30 percent leading to higher efficiency and translating into lower case temperature, giving designers options for improving overall system performance and reliability. Optimized for targeted applications, these devices show a reduction in case temperature of up to 20 percent over existing devices.

“An increase in the number of electrical appliances in use has led to a steady rise in the total energy consumption within the growing industrial and consumer markets,” said Paul Leonard, vice president and general manager for ON Semiconductor’s Power Discrete products. “ON Semiconductor’s continued development into thin wafer processing and implant technology allows for significant improvement in IGBT performance that is critical to support the increasing need for energy efficient solutions.”

The first group of FSII IGBTs is the NGTBxxN120IHRWG and NGTBxxN135IHRW; these devices feature optimized switching and reduced conduction losses for induction heating and soft switching applications operating at medium frequencies of 15 kilohertz (kHz) to 30 kHz. With excellent ruggedness and superior on-state characteristics at high currents, these devices are optimized, based on system requirements to enable higher efficiency and lower system losses. These high-speed IGBTs are providing industry leading system level performance in induction heating based products such as hot pots, rice cookers and microwave appliances. The family of devices is available in both 1200 volt (V) and 1350 V platform versions with current ratings of 20 amperes (A), 30 A and 40 A.

Further expansion of the FSII IGBT technology includes the NGTBxxN120FL2WG and NGTBxxN135FL2WG family of devices designed specifically for solar inverter, uninterrupted power systems (UPS), and inverter welder applications. With improved thermal characteristics, these new devices will have an operational junction temperature range of -55 to +175°C and increase in current ratings up to 100 A in TO-247 packages.

ON Semiconductor has a track record of quality and reliability in IGBTs with automotive AEC-Q qualified IGBT’s in production for more than a decade. In 2011, the company started new development in high-voltage/high-current devices for the growing industrial and consumer marketing, which continue to demand high efficiency solutions. The first full portfolio family of the company’s proprietary Trench Field Stop technology was released in 2012 matching competitive technology. The release of this newest FSII IGBT technology puts the company in a leading market position.

PCIM - ON Semiconductor Booth - Hall 9, Stand No. 550

ON Semiconductor will be featuring live product presentations for power discrete IGBTs for induction heating, efficient motor drive and solar inverters at PCIM from May 14-16 at Stand 550 in Hall 9 of the Exhibition Centre Nuremberg.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.