ON Semiconductor Introduces a Comprehensive Array of New Medium Voltage N-Channel MOSFETs

Optimized for reducing switching, conduction & driver power losses to boost efficiency















New Medium Voltage N-Channel MOSFET

PCIM - Nuremberg, Germany. – May 19, 2015 – ON Semiconductor (Nasdaq: ON), ON Semiconductor (Nasdaq: ON), driving energy efficiency innovations, has further expanded its broad portfolio of power MOSFETs with new, high efficiency single n-channel devices targeted at data networking, telecommunications and industrial applications.

These devices are capable of delivering incredibly low on state resistance, RDS(on), values, thereby minimizing conduction losses and improving overall operational efficiency levels. They also have very low gate capacitance (Ciss) - down to 2164 picofarads (pF) - which ensures driver losses are kept as low as possible.

With a rated breakdown voltage of 40 volts (V), the company’s new NTMFS5C404NLT, NTMFS5C410NLT and NTMFS5C442NLT MOSFETs have maximum RDS(on) values (@ Vgs = 10 V) of 0.74 milliohms (mΩ), 0.9 mΩ and 2.8 mΩ respectively, with continuous drain currents of 352 amps (A), 315 A and 127 A respectively. These are complemented by the NTMFS5C604NL, NTMFS5C612NL and NTMFS5C646NL, all of which have breakdown voltage ratings of 60 V. The maximum RDS(on) of these devices is 1.2 mΩ, 1.5 mΩ and 4.7 mΩ respectively, while their associated continuous drain currents are 287 A, 235 A and 93 A. Both the 40 V and 60 V devices are rated to operate at junction temperatures up to 175 ˚C, thereby giving engineers greater thermal headroom for their designs. ON Semiconductor will be expanding this offering with devices which feature additional RDS(on) values and different packages, such as micro8FL, DPAK and TO220.

“Engineering teams at OEMs are constantly striving to create power system designs that are capable of attaining higher degrees of efficiency while simultaneously taking up less board space,” said Paul Leonard, vice president and general manager for ON Semiconductor’s Power Discrete Products. “With these new additions to our extensive power MOSFET offering, we are providing customers with high performance devices, in compact thermally efficient packages, that will help them to achieve this goal.”

Packaging and Pricing

The NTMFS5C404NL, NTMFS5C410NL, NTMFS5C442NL NTMFS5C604NL, NTMFS5C612NL and NTMFS5C646NL are all offered in compact, RoHS-complaint SO8FL (DFN-8) packages with pricing starting at $0.42 per unit in 10,000 unit quantities.

Visit ON Semiconductor at PCIM 2015 – Hall 9, Stand 559

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.