ON Semiconductor Expands into High Performance, High Density Power Integrated Module (PIM) Market

Pushing the power efficiency envelope while maintaining reliable operation and simplifying system development















High Performance, High Density Power Integrated Modules

PCIM - Nuremberg, Germany. – May 19, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficiency innovations, has introduced a state-of-the-art 80 ampere (A) Power Integrated Module (PIM) with industry leading performance for demanding uninterruptable power supplies (UPS), industrial variable frequency drives, and solar inverter applications.

Leveraging ON Semiconductor’s proprietary Trench Field Stop II technology along with rugged ultrafast fast recovery diodes, the NXH80T120L2Q0PG PIM module is configured in 1200 volt (V), 80 A half-bridge and 600 V, 50 A neutral point clamp T-type topology, attaining efficiencies in excess of 98 percent. The configurable package platform employs high-power direct-bonded-copper (DBC) substrate technology along with proprietary press-fit pins to provide customers with a high performance and reliable power module solution.

ON Semiconductor’s expansion into the PIM market is rooted in more than 30 years of experience in automotive ignition IGBTs and intelligent power module (IPM) development. The NXH80T120L2Q0PG PIMs employ ON Semiconductor’s extensive packaging expertise, and are fully qualified to the highest industry standards for reliability at junction temperatures (Tj) of 175°C. In addition, ON Semiconductor module solutions provide customers with a fully-integrated supply chain for silicon and packaging, ensuring high quality and cost efficiencies.

“Power integrated modules are an integral part of our Power Vision to expand into higher power industrial and automotive markets,” said Paul Leonard, vice president and general manager for ON Semiconductor’s Power Discrete Products. “This new, extremely rugged, power module platform is a continuation of our commitment to provide a full portfolio of power discrete and module solutions, enabling our customers to meet their needs for high efficiency, high density power solutions.”

Packaging and Pricing

The NXH80T120L2Q0PG is available in Q0PACK packages (measuring 65.9 mm x 32.5 mm x 11.75 mm). Pricing starts at $30.00 per unit in 1,000 unit quantities.

Visit ON Semiconductor at PCIM 2015 – Hall 9, Stand 559

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.