ON Semiconductor Expands Building Automation Portfolio with Three New High-Efficiency KNX Transceivers

October 06, 2015

NCN5110, NCN5121 and NCN5130 transceivers boost available power for external loads, help designers create compelling smart-building systems















KNX certified high efficiency twisted pair transceivers

Intelligent Building Systems (IBS) Conference – Booth F26 - PARIS, France – Oct. 6, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced three new KNX certified twisted pair transceivers for smart building applications. The new devices allow small, low-cost external components, while delivering increased regulator current and boosting overall efficiency by up to 20 percent compared to existing solutions.

“The three new transceivers we are launching today support the world‘s most adopted standard for building automation, and enable designers to create even more cost-effective products offering greater functionality and energy efficiency,” said Ryan Cameron, vice president of Industrial and Timing products for ON Semiconductor. “Making buildings smarter is key to preserving the environment and ensuring energy security, as buildings currently represent about 40 percent of the world’s energy consumption.”

The NCN5110, NCN5121 and NCN5130 integrate two high-efficiency DC-DC converters and a 20 V low drop-out regulator for powering external loads from the bus. The devices are offered in a QFN-40 package and are specified for operation over the extended temperature range of -40°C to 105°C.

The NCN5121 and NCN5130 implement the complete KNX physical (PHY) and media-access (MAC) layers, while the NCN5110 is an analog-only bit transceiver to be used in combination with a microcontroller hosting the KNX MAC. The NCN5121 is pin to pin compatible with NCN5120, and offers higher efficiency and increased regulator output. As ON Semiconductor’s most advanced transceiver, the NCN5130 is capable of taking up to 40 mA from the KNX Bus, which is the highest current on the market, and gives designers greater flexibility to power devices such as an LCD panel or touchscreen, or for driving relays at higher speeds.

The new devices allow designers to specify lower external capacitance and inductance values. Compared to other transceivers on the market, this can yield savings up to 40 percent. In addition, the smaller values translate into physically smaller component sizes. In combination with the highly compact package size, this saves board space and enables designers to satisfy the tough space constraints typical of many KNX applications.

About KNX

KNX Association is the creator and owner of the KNX technology – the worldwide STANDARD for all applications in home and building control, ranging from lighting and blind control to various security systems, heating, ventilation, air conditioning, monitoring, alarming, water control, energy management, smart metering as well as household appliances, audio/video and many more. KNX provides a single, manufacturer independent design and commissioning tool (ETS), with a complete set of supported communication media (TP, PL, RF and IP) as well as a complete set of supported configuration modes (system and easy mode). KNX is approved as a European (CENELEC EN 50090 and CEN EN 13321-1) and an International standard (ISO/IEC 14543-3). This standard is based upon 25 years of experience in the market. Over 400 member companies worldwide from different application domains have more than 7000 KNX certified product groups in their catalogues. The KNX Association has partnership agreements with almost 50,000 installer companies in more than 125 countries. For more information, visit https://www.knx.org.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy