ON Semiconductor Announces New Solutions Enabling State-of-the-Art Wireless and Recharging Features in Hearing Aids

PHOENIX, Ariz. – October. 20, 2015 –

Share

Latest Signal Processing & Power Management Devices for User Friendly, State-of-the-Art Hearing Aids















Ezairo 7150 SL wireless-enables audio processor hearing aids.

PHOENIX, Ariz. – October. 20, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, further underlines its leadership position in assisting next generation hearing aid development with the introduction of two new products: HPM10, a Power Management Integrated Circuit (PMIC); and Ezairo® 7150 SL, a wireless-enabled audio processor.

Ezairo® 7150 SL uses the company’s widely-implemented proprietary digital signal processing (DSP) technology and brings wireless connectivity to hearing aids and cochlear implants. The compact hybrid module is based on the powerful Ezairo 7100 open-programmable 24 bit mixed-signal DSP platform. This System in Package (SiP) solution provides wireless multi-protocol operation and is optimized for 2.4 gigahertz (GHz) band applications, including Bluetooth® Low-Energy (BLE). Ezairo® 7150 SL integrates EA2M, a low power 2 Mb serial CMOS EEPROM used for storing hearing aid firmware and important parameters.

To simplify and accelerate the development process of an Ezairo® 7150 SL-based product, ON Semiconductor has provided a complete reference design of a behind-the-ear (BTE) hearing aid. The reference design includes software, hardware, and firmware which enable advanced wireless features. The control over BLE (CoBLE) function allows hearing aid users to control an array of parameters from their smartphone. The user can adjust the hearing aid’s volume, make program changes, check the battery status, and receive phone alerts (such as incoming calls or text messages). It also features a valuable ‘Find Me’ function to help users quickly locate a misplaced hearing aid. The stereo audio streaming proprietary protocol enables music to be streamed from any external audio source (smartphones, tablet computers, televisions, etc.) through a remote dongle. The connectivity range can reach up to 10 meters in good surrounding conditions.

HPM10 is a Power Management IC (PMIC) that provides a high−performance solution for rechargeable batteries in hearing aids and hearing implant devices. The PMIC generates the voltage needed by the hearing aid and it also manages the charging algorithms such that the battery autonomy and the number of charging cycles are optimized. The rechargeable chemistries supported include silver−zinc (AgZn), and lithium−ion (Li−ion). HPM10 also detects zinc−air (Zn−Air) and nickel metal hydride (Ni-Mh) batteries but doesn’t charge them.

During operation, HPM10’s high efficiency power regulators help minimize lost power from the battery to the hearing aid. HPM10’s built-in charger communication interface (CCIF) can pass data to the hearing aid charger during the charging process. Battery parameters such as voltage levels, current levels, temperature and different forms of battery failures can also be communicated. Different charging parameters, representative of battery size and type, can be stored in the HPM10’s on-chip one-time programmable (OTP) memory.

“Our new solutions are set to have real impact on hearing aid design and the end-user experience. Ezairo® 7150 SL allows much improved user control over their device directly from any BLE-enabled smartphone. It also allows users to listen to audio from any source, like televisions or HiFi audio systems,” states Michel De Mey, senior director at ON Semiconductor. “By enabling rechargeable technology in hearing aids, HPM10 helps answer the need of our customers and the market to provide rechargeable hearing aids, which is another great step towards increased user friendliness.”

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.