ON Semiconductor Announces High Performance System-in-Package (SiP) Solution for Precision-Sensing in Portable Medical Devices

September 15, 2014

Semi-customizable, power efficient SiP solution enables miniature sensing systems ideal for mHealth applications including glucose monitors, heart rate monitors, and electrocardiogram analyzers















Struix High Performance System-in-Package (SiP) Solution for Precision Sensing in Portable Medical Devices.

PHOENIX, Ariz. – Sept. 15, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has responded to rapidly-evolving product development demands within the portable medical market by introducing Struix, a semi-customizable System-in-Package (SiP) solution for precision sensing and monitoring in a variety of mobile medical electronics including glucose monitors, heart rate monitors and electrocardiogram analyzers.

Struix, which means “stacked” in Latin, utilizes advanced die stacking technology to integrate a custom-designed analog front-end (AFE) on top of an industry-leading 32-bit Application Specific Standard Product (ASSP) microcontroller (ULPMC10), to form a complete miniature system. By using standard and customizable components, Struix offers medical device manufacturers the design flexibility required to create unique medical sensor interface applications while improving time-to-market and cost-effectiveness.

“Advanced stacking technology enables Struix to achieve greater system integration and occupy less board space in medical devices than standalone solutions,” said Michel De Mey, senior director of consumer health solutions at ON Semiconductor. “ON Semiconductor’s SiP approach reduces design time, development risks and the costs associated with fully customized solutions. Design flexibility is further enhanced because the solution’s ULPMC10 microcontroller can be easily updated with future microcontrollers from ON Semiconductor, without replacing the AFE, which is subject to FDA re-certification.”

The ULPMC10 microcontroller element of Struix processes signals using an industry-leading 32-bit ARM® Cortex®-M3 core capable of running up to frequencies of 30 megahertz (MHz). The microcontroller incorporates 512 kilobytes (kB) on-chip Flash memory and 24 kB SRAM memory to store critical program and user data. Designed to improve battery life in portable devices, ULPMC10 offers superior performance with minimal dynamic and static power demands. Through on-chip charge pump-based power conversion and regulation, the microcontroller can operate at a current consumption of less than 200 µA/MHz. While in standby mode, current consumption remains below 500 nanoamperes (nA), a critical parameter for low-duty cycle medical devices.

The system’s advanced power management subsystem monitors the device for fail-safe operation with a wide variety of battery voltages without requiring external components. The microcontroller also includes a12-bit analog-to-digital converter with three multiplexed inputs, a real-time clock, a phase-locked-loop, and a temperature sensor. To simplify product development, ON Semiconductor offers a comprehensive and easy-to-use suite of development add-ins for IAR Systems to support the ULPMC10 microcontroller, including CMSIS based software interfaces.

Using ON Semiconductor’s custom chip engagement model, medical device manufacturers can take advantage of an extensive portfolio of intellectual property and design experience to meet the stringent feature and performance- level requirements of medical sensor applications.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.