ON Semiconductor&#153 Adds TTL Compatible Functions to VHC Portfolio

Share

Phoenix, AZ - June 16, 2000 - ON Semiconductor (Nasdaq: ONNN) has continued the expansion of the VHC logic portfolio to include eight new TTL compatible functions. These devices which include NOR, AND, OR, XOR and Bus functions, offer equivalent performance and full pin compatibility with existing non-TTL functions in the series and competitive AHC devices.

These new functions are advanced high-speed CMOS functions fabricated with silicon gate CMOS technology. They achieve high-speed operation similar to equivalent Bipolar Schottky TTL while maintaining CMOS low power dissipation. They offer designers an easy transition from 5 volt systems to mixed 3 volt / 5 volt systems with functions that offer speed, drive and power performance advantages. Typical gate propagation delays for the functions are well below 4 nsec and the VHCT inputs are compatible with TTL levels. All the devices can be used as level converters for interfacing 3.3 volt to 5 volt, because they have full 5 volt CMOS level output swings.

"VHC is a very high-speed CMOS logic family that provides a natural migration path for HCMOS (MC74HCXXX) users requiring higher speed, lower power and low-drive products. Expanding the VHC portfolio demonstrates our continuing commitment to providing legacy logic families," said Jess Diaz, Market Development Manager for Standard Logic Business Unit at ON Semiconductor. "ON Semiconductor's advanced 0.6micron process produces high performance basic gates, octal and 16-bit functions at lower costs."

The new additions to the VHC family include the MC74VHCT02A Quad 2-Input NOR Gate, the MC74VHCT08A Quad 2-Input AND Gate, the MC74VHCT32A Quad 2-Input OR Gate, the MC74VHCT86A Quad 2-Input XOR Gate, the MC74VHCT125A Quad Bus Buffer, the MC74VHCT126A Quad Bus Buffer, the MC74VHCT132A Quad 2-input NAND Schmitt Trigger and the MC74VHCT540A Octal Bus Buffer. All the functions in the portfolio are ideal for general-purpose logic applications in virtually all market segments.

Along with the other functions in the portfolio, these devices have 5 volt tolerant inputs, power down protection on the inputs, low noise of VOLP of 0.8 volts, a 2 volt to 5.5 volt power supply range, a maximum static current of 20 5A and latch-up performance exceeding 300 mA.

The MC74VHCT02A, T08A, T32A, T86A, T125A, T126A, and T132A are available in 14 pin SOIC and TSSOP packages. The T540A is available in both 20-pin SOIC and TSSOP packages. Pricing is suggested in the range of $0.12 to $0.32 per 2.5K unit quantities. Samples and production quantities are currently available. For more information on ON Semiconductor's VHC devices, visit VHC Logic Family

About ON Semiconductor

ON Semiconductor, formerly a division of Motorola, is one of the world's largest suppliers of analog, standard logic, and discrete semiconductors for data and power management. ON Semiconductor's products include integrated circuits for high-bandwidth data applications, analog ICs for power management and low-voltage power transistors. In addition to using micropackaging technology across all product families, ON Semiconductor offers the largest selection of discrete semiconductors in a variety of surface mount and standard packages. These semiconductors turn on and connect digital electronic products to our world. ON Semiconductor is the trade name of SCG Holding Corporation's affiliate, Semiconductor Components Industries, LLC.

# # #

Motorola is a registered trademark of Motorola, Inc.

Photo available through Editorial contact.

For more information:

Yinka Massally
Media Relations Manager
ON Semiconductor
602-244-6398
Linda Capcara
Group Manager
Brodeur Worldwide
602-282-5427

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.