ON Semiconductor Addresses High Demand for Low Power, Integrated Wireless Devices to Drive Connectivity of the Internet of Things

November 03, 2014

New standards compliant NCS3651x family of system-on-chip (SoC) transceivers support communications for the IoT and smart metering















2.4 GHz ultra-low power transceiver.

European Utility Week – AMSTERDAM, Netherlands – Nov. 3, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, is using this year’s European Utility Week Exhibition and Conference as the forum to launch an important new product family that supports high-performance, reliable and efficient communications for the Internet of Things (IoT) and smart metering applications. The NCS3651x family of system-on-chip (SoC) transceivers has been developed using ON Semiconductor’s expertise in highly integrated mixed signal integrated device technology and radio frequency (RF) design. The company is also an active member of the ZigBee® Alliance.

The NCS3651x is a family of 2.4 gigahertz (GHz) ultra-low power wireless transceivers based on the IEEE 802.15.4-2006 standard which support protocols such as ZigBee, 6loWPAN, WirelessHART, and proprietary versions. These solutions are ideal for use in low data rate, intermittent communication IoT applications in smart metering and consumer appliances. All devices are optimized for low power consumption and high efficiency with single supply operation from a standard battery (1.0 volt (V) to 3.6 V) and best in class low receive and transmit currents. This enables growing market demands for alternative energy solutions such as energy harvesting. It also expands support for additional battery types while dramatically increasing battery life.

The NCS3651x incorporates a powerful 32-bit ARM® Cortex®-M3 processor as well as various configurations of RAM for data storage and FLASH memory for program storage. This includes a best-in-class full memory configuration which will allow customers to support multiple application and software protocols. Multiple peripherals enable the design of a complete wireless network with a minimum of external components.

“Low-power, robust, integrated wireless communications devices will be key in helping the Internet of Things and smart metering achieve their huge and exciting potential,” said Ryan Cameron, vice president of Industrial and Timing products for ON Semiconductor. “At ON Semiconductor we have proven experience working on RF wireless device designs. This combined with our extensive mixed-signal and integration expertise has allowed us to develop and launch some truly enabling communications products that deliver low power consumption and high performance.”

Packaging and Pricing

The NCS3651x family is currently sampling to early adopters with volume production expected in early to mid-2015. The new devices are housed in space saving QFN-40 RoHS-compliant packages.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.