Advanced Audio-Processing SoC from ON Semiconductor Delivers Superior Experiences on Mobile Devices

October 27, 2015

Dual-core processing architecture with hardware acceleration and available software modules reduces development time, saves board space and boosts battery life















Advanced Audio Processor from ON Semiconductor

PHOENIX, Ariz. – October 27, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has released its latest high-resolution audio processing System-on-Chip with 1656KB SRAM and power-efficient hardware acceleration, bringing extra space savings and longer battery life to devices such as smartphones, wearable accessories and voice recorders.

Powering the LC823450 are a highly efficient ARM® Cortex®-M3 core and ON Semiconductor’s 32-bit/192kHz audio-processing engine with hardware-based MP3 encoding/decoding and wireless-audio support, which boosts performance and power efficiency. In addition, a large selection of royalty- and license-free DSP code samples are available, which help accelerate software design and minimize development costs. These include advanced functions such as noise canceller, and S-Live (Low-frequency Intelligence Virtual Excitation) for enhanced playback of low frequencies.

With its generous on-chip SRAM, the new LC823450 has plentiful memory for audio processing and application tasks without needing a companion memory chip. Designers can also take advantage of rich integrated audio peripherals, such as an analog/digital converter, phase-locked loop and class-D amplifier. In addition, industry-standard interfaces such as SPI, I2C, SDCard and UART enable product designers to build in versatile connectivity.

“High-resolution audio takes listening pleasure to a new level, and our new LC823450 delivers superior experiences on mobile devices through class-leading integration and power efficiency,” said Atsushi Bando, General Manager of the ON Semiconductor, System Solutions Group. “Rich integrated features, hardware acceleration and easy software terms also make life easier for product developers by helping manage development costs and minimize time to market.”

Packaging and Pricing

The Pb-free LC823450 is packaged in a compact 5.52 mm x 5.33 mm WLP-154 that reduces footprint by up to 85% over competing solutions, and is priced at $8.34 per unit in 1,000 unit quantities. The device is also available in a TQFP-128L, priced at $8.00 per unit in 450 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.