ON Semiconductor Introduces Integrated Linear Current Regulator and Controller for Automotive Lighting

New device allows engineers to develop more sophisticated lighting control systems through simple programming of discrete LED brightness levels

Linear Regulator and Controller Image

PHOENIX, Ariz. –June 2, 2010– ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics has announced the release of a linear regulator and controller product. The NCV7680 consists of eight linear programmable constant current sources. It is designed for use in the regulation and control of solid state rear combination lamps of vehicles, and is capable of supporting an LED driving current of up to 75 mA per channel. 

Due to its high degree of integrated functionality, the NCV7680 allows support for two brightness levels - one for stop and one for tail illumination. Optional pulse width modulation (PWM) control can also be implemented if required. System designers can set the output current (global set point) with the use of just one external resistor. An optional external ballast FET allows for power distribution on designs requiring high currents.

Qualified to the AEC Q100 automotive standard, the NCV7680 has a MSL 1 moisture resistance rating, and an operating temperature range of −40 ⁰C to +150 ⁰C. Typical applications for this device include rear combination lamps, daytime running lights, fog lights, center high-mounted stop lamp arrays, turn signal lamps and LCD backlighting.

“Automotive lighting systems are now expected to be more feature rich, and this requires the employment of highly integrated solutions which provide superior current regulation,” said Andy Williams, senior vice president, Automotive Power Group, ON Semiconductor. “The release of the NCV7680 takes care of powering rear combination lamps in a single chip, delivering enhanced performance and higher levels of efficiency, in a smaller footprint than existing solutions on the market. It also allows better matching of LED outputs than would be possible with a discrete solution, as well as enabling fault identification.”

Packaging and Pricing

The NCV7680 is offered in a SOIC-16 Pb−free package. Pricing for these devices is $1.70 per unit in 10,000 unit quantities.

For more information, please visit https://www.onsemi.com

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.