ON Semiconductor Introduces All-in-One Auto Focus Controller for Smartphone Camera Modules

Integrated solution delivers high performance auto focusing as well as lower power consumption















LC898214XC Auto Focus Controller.

PHOENIX, Ariz. – July 16, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has introduced the LC898214XC Auto Focus Controller for camera modules in smartphones.

This integrated solution features digital loop filter and provides fast, accurate auto focus convergence with temperature compensation, while consuming minimal power. The integrated constant current driver provides lower electro interference noise than competing solutions. In addition, the space-saving design enables thinner and lighter smartphones.

“There is a strong and growing demand for improved smartphone camera features – specifically for fast, accurate, power-friendly auto-focus,” said Ikuya Kawasaki, general manager of the Intelligent Power Solution division at ON Semiconductor. “We developed this highly integrated, all-in-one auto focus controller for the specific demands of smartphone applications. The market demands higher performance auto focusing, with low power consumption and small size. The LC898214 provides the desired accuracy with a closed auto focus system.”

LC898214XC integrates all functions for the closed auto focus driver, including digital logic as a closed auto focus control, Hall device as a positioning sensor, EEPROM for the storage of filter parameters and compensation data, and a constant current driver as an actuator driver. The closed auto focus system provides for more accurate auto focus control, while also lowering power consumption compared with open loop systems. The loop filter coefficients are adjustable via an I2C interface, allowing the device to be programmed for optimal convergence time when paired with various different actuators. These integrated features support a closed auto focus system, and can provide higher auto focus performance from one integrated circuit.

Packaging and Pricing

LC898214XC is offered housed in a Pb-free, Halide-free WLCSP-8 package and is priced at $0.88 USD per unit in quantities for 4,000 units.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.