ON Semiconductor Announces Sensorless Three-Phase Motor Controller for Automotive BLDC Implementation

Highly integrated solution, including BLDC commutation and gate drivers, eliminates need for microcontroller unit

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
 LV8907UWWeb

PHOENIX, Ariz – June.20, 2016 – ON Semiconductor (Nasdaq: ON ), has further expanded its portfolio of motor controllers with the introduction of the LV8907UW. Supporting an operating voltage range from 5.5 to 20 volts (4.5 to 40 V transient), this high performance and feature-packed device enables streamlined three-phase brushless DC motors. The LV8907UW integrates gate drivers for six N-channel MOSFETs, and a dual-stage charge pump for 100% duty-cycle operation. In its lowest cost configuration the IC can operate without an external microcontroller. The device requires no programming, as key parameters and functions - such as startup and speed setting - can be configured via SPI interface and stored in embedded non-volatile (OTP) memory. Open-loop and closed-loop speed control are possible. For more complex applications the LV8907UW can also support a small microcontroller with its integrated linear regulator (3.3V or 5V, 50mA), a local interconnect network (LIN) transceiver for automotive connectivity, and a watchdog timer.

AEC-Q100 qualified, the LV8907UW’s operational temperature range reaches up to 175°C, thereby ensuring reliable operation in challenging automotive environments. Integrated protection mechanisms include over-current, over-voltage, short circuit, under-voltage, and over-temperature. The features of the device make it ideal for use in automotive water pumps, oil pumps, fuel pumps, HVAC systems, radiator fans, and headlamp cooling units.

“Compelled by market pressures and increasingly stringent legislative measures, automotive manufacturers need to find ways to improve the fuel economy of their models. Electrification of former mechanical applications – such as pumps and fans – is a key step in this path”, explains Ikuya Kawasaki, General Manager of System Solutions Group at ON Semiconductor. “Thanks to its high degree of integration and support for sensor-less operation, the LV8907UW enables motor systems to attain maximum efficiency levels without a microcontroller. The resulting designs have reduced complexity and bill of materials, and enhanced reliability.”

Packaging and Pricing
The LV8907UW is supplied in a SQFP48K package format. It is priced at $5.55 per unit in 2,500 unit quantities.