PHOENIX, Ariz. – May 2, 2017 –

Share

Collaboration between ON Semiconductor and RFMicron leads to effective leak detection system to improve outgoing vehicle quality, and alleviate risk of related latent malfunction and customer warranty issues

PHOENIX, Ariz. – May 2, 2017 – ON Semiconductor (Nasdaq: ON) and RFMicron have expanded their collaboration to develop a complete in-line vehicle production leak detection solution. The RFM5126 Moisture Intrusion Detection System uses battery-free, wireless sensors to detect in-vehicle water leaks caused by incorrect assembly. Detecting leaks and assembly issues before a vehicle leaves the factory is critical to improving outgoing quality and to avoiding customer warranty issues. The new automated leak detection system, assembled in the production line, enables detection of the smallest damage-inducing leaks.

The system employs moisture detection sensors that incorporate Magnus® IC from RFMicron. Magnus-based IC supports a revolutionary range of battery-free wireless sensors offered under Smart Passive Sensors™, and SPS™.

Vehicle assembly is a complex process involving a range of materials, glues, changing components and human-driven processes. Even with the best traditional efforts, small leaks can go undetected during manual inspection procedures. These leaks may allow enough water into the vehicle over time to cause mold growth and potential damage to expensive electronics modules and components. Statistics show that up to 3% of vehicles ship from the factory with leaks that will lead to mold growth and costly warranty repairs. The RFM5126 Moisture Intrusion Detection System is able to accurately identify these leaks with lower cost and labor impact versus traditional and less effective methods.

The unobtrusive, battery-free, wireless sensors are installed in the vehicle at the bare metal stage before installation of the interior trim and seats. After completing all assembly, vehicles move through a high-pressure spray test where the system flags any small, hard-to-find leaks. Drive-through portal stations that are easily installed on existing vehicle assembly lines, facilitate communication with the sensors. The portal stations incorporate comprehensive sensor monitoring software that reports accurate leak locations helping to speed the rework process. Over time, the system strengthens process improvement efforts by helping automakers identify issues that lead to leaks in the first place.

“Automakers can already detect the major leaks which tend to be visible, but they have great difficulty detecting small leaks which cause damage over an extended period of time,” said Shahriar Rokhsaz, CEO, RFMicron. “The RFM5126 Moisture Intrusion Detection System identifies nearly all mold-causing small leaks and a large majority of ‘micro leaks’. Our objective is to catch the small leaks before vehicles leave the factory. Our battery-free wireless sensors, and our associated software, provide a highly effective and cost-efficient solution to make this happen.”

“Hard to detect leaks are a significant issue for automakers,” said Gary Straker, Vice President of the Protection and Signal Division at ON Semiconductor. “This new system automatically detects very small leaks on the assembly line, giving the opportunity to address the root causes of the problem and make process changes to improve outgoing quality. As an added benefit, repairs at the factory are lower cost since the right materials and fully trained personnel are on-hand. Finding leaks and dealing with them earlier, combined with major reductions in repair costs, and the avoidance of any impact on an automaker’s reputation for quality, gives an attractive potential return on investment for the industry.”

For more details, please read the white paper titled Moisture Intrusion Detection System: “Solving Water Leak Inspection Challenges on Vehicle Assembly Lines”. Visit the website”, watch the videos”, and learn more about battery-free wireless sensor technology.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.