Power Solutions from ON Semiconductor
Contact Us | Company | Investors | Careers
 
         
 
Print

ON Semiconductor Introduces its Fourth GreenPoint™ Power Supply Reference Design – Again Delivering Profound Energy Efficiency

New 220 watt LCD-TV power supply solution delivers standby power of less than 1 watt

Applied Power Electronics Conference (APEC) – Dallas, TX – March 20, 2006 – ON Semiconductor (Nasdaq: ONNN), a leading global supplier of power management solutions, today unveiled its fourth GreenPoint™ reference design – this one for 220 watt (W) LCD-TV power supplies. Like the CRT-TV open reference design the company introduced earlier in the month, this flat-screen television design delivers standby power of less than 1 W, addresses all functional blocks of the power supply, and meets international regulations for low standby power dissipation.

“The LCD-TV, CRT-TV, ATX and notebook adapter power supply reference designs that ON Semiconductor has successfully developed, built and fully tested during the past year, demonstrate our ongoing dedication to deliver industry-leading, energy efficient, power sources,” said Andy Williams, vice president of ON Semiconductor’s Power Conversion Products Division. “These open reference designs help electronics manufacturers tighten their design cycles and deliver competitive consumer products with reduced energy waste.

“While developing our GreenPoint™ power solutions,” said Williams, “we work closely with our worldwide customers to assure the creation of effective solutions that directly address present and future power needs. ON Semiconductor plans to continue to deliver ‘green’ solutions that ease the design burden on our customers for increasingly efficient power supplies.”

The Reference Design To achieve breakthrough performance, the new LCD-TV GreenPoint™ reference design utilizes several of ON Semiconductor’s advanced power management devices and draws from the company’s industry-leading discrete component portfolio.

The enabling devices for the LCD-TV reference design are the newly introduced NCP1395 and NCP5181.
• NCP1395 – a high performance resonant mode controller that offers everything needed to build a reliable and rugged power supply. Its unique architecture includes a 1.0 megahertz (MHz) Voltage Controller Oscillator and protections featuring various reaction times that contribute to a safer converter design, without engendering additional circuitry complexity. This device is offered in an SOIC-16 package, priced at $1.38 per unit in 2,500 unit quantities, and a PDIP-16 package, priced at $1.50 per unit in 500 unit quantities.

• NCP5181 - a high voltage power MOSFET driver that provides two outputs to drive two N-channel MOSFETs. The NCP5181 uses the “bootstrap” technique to ensure proper drive of the high-side power switch. This device is offered in an SOIC-8 package, priced at $1.60 per unit in 2,500 unit quantities, and a PDIP-8 package, priced at $1.74 per unit in 1,000 unit quantities.

Other key devices include:
• NCP1653 - a compact Power Factor Correction (PFC) controller that is ideal for continuous conduction mode (CCM) PFC applications like those found in flat-screens televisions. This device makes the choice of incorporating a PFC front-end into a power supply design easy by reducing part count and providing a robust, cost-effective front-end without range switches. This device is offered in an SOIC-8 package, priced at $0.80 per unit in 2,500 unit quantities, and a PDIP-8 package, priced at $0.88 per unit in 1,000 unit quantities.

• NCP1027 – a highly integrated Switch Mode Power Supply (SMPS) switcher. This device provides improved efficiency at light loads by entering a skip cycle when power demand is low. This device is offered in a PDIP-8 package, priced at $0.95 per unit in 1,000 unit quantities.

Supporting devices include:
• TL431 – a programmable precision reference.
• MBR10H100CT – 100 V, 10 A, H-series SWITCHMODE™ power rectifier.
• MBRS260 – 60 V, 2 A, schottky power rectifier.
• MMSZ7V5E - 225 W, 7.5 V, energy rated zener.

A complete documentation package for the LCD-TV power supply is available - including description, schematic, bill-of-materials, Gerber images, and evaluation results. These materials are available at www.onsemi.com, as are the product specifications and other supporting information.

About GreenPoint™
GreenPoint™ is ON Semiconductor’s family of high-efficiency power supply reference designs that meet existing or emerging energy efficiency standards. GreenPoint™ reference designs are available for an ATX power supply, a CRT-TV power supply, an LCD-TV power supply and a notebook adapter. To acquire documentation packages for these designs, visit www.onsemi.com and run a keyword search on “GreenPoint”.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at http://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.