TOKYO, Japan – TECHNO-FRONTIER - July 22, 2014 –

Share

LC05111CMT helps reduce charging time of portable electronics with high-precision control of charge/discharge current















LC05111CMT Lithium-ion battery protection controller.

TOKYO, Japan – TECHNO-FRONTIER - July 22, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has announced a new Lithium-ion battery protection controller for smartphones and tablets. The highly-integrated LC05111CMT utilizes analog circuit technology, MOSFET technology, and advanced packaging expertise to incorporate controller and driver functions in a single circuit.

The LC05111CMT enables high-precision current control without using a current detection resistor. This current control reduces charging time by enabling higher charging current. The device includes highly accurate detection circuits and detection delay circuits, to prevent batteries from over-charging, over-discharging, over-current discharging, and over-current charging. The high level of integration reduces component count and therefore required board space in the space-constrained battery pack.

“There is a clear requirement for the more accurate battery current control and small package in advanced portable devices,” said Ikuya Kawasaki, general manager of the Intelligent Power Solution division at ON Semiconductor. “The LC05111CMT combines technologies to deliver a physically small, yet functionally innovative device that helps reduce charging time and provides multiple levels of protection for the battery charging circuit.”

Packaging and Pricing

LC05111CMT is offered in a Pb-free and Halide-free WDFN-6 package, and is budgetary priced at $1.00 USD in quantities of 10,000 units.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.