ON Semiconductor Introduces Fully Integrated Li-Ion Battery Charger to Address Next Generation Power Efficiency Demands

PHOENIX, Ariz. – Aug. 27, 2012 –

Share

Programmable device provides faster charging, improves battery life in portable electronics

1381_NCP1851 Fully Integrated Li-Ion Battery Charger

PHOENIX, Ariz. – Aug. 27, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has introduced a fully programmable Lithium- Ion (Li-Ion) switching battery charger optimized for power efficiency in smart phones, tablets and other handheld devices. The NCP1851 significantly reduces charge time, increases battery life and includes advanced startup features.

With 1.6 ampere (A) charging capability, the device is perfectly sized at 2.2 x 2.55 mm for the latest USB compliant input supplies and large battery capacities and can complete a full charge cycle of a 1650 milli ampere hour (mAh), 4.2 volt (V) Li-Ion battery in 90 minutes.

“Robustness, efficiency and fast charge time are now pre-requisites for designers of today’s high performance, ultra-space constrained applications,” said Thibault Kassir, director of ON Semiconductor’s Interface & Power ICs Division. “The NCP1851 single chip solution allows simple integration into the latest USB charging designs. We are already receiving wins from our major customers for the device due to its charge time performance and advanced feature set.”

The NCP1851 integrates dynamic power path management which enables instant system turn-on in case of a weak battery and helps replenish a deeply discharged battery. Both the device’s internal junction temperature sensor and external Negative Temperature Coefficient (NTC) thermistor ensure safe charging of the system by reporting dedicated interrupts to the i²C Control Bus. The NCP1851 provides a USB On-the-Go (OTG) mode that boosts battery voltage to power accessories plugged into the USB port, eliminating the need for another step-up converter.

Packaging and Pricing

The NCP1851 is housed in a 25 bump Flip-Chip CSP package case with overall dimensions of a mere 2.2 mm x 2.55 mm and height of 0.6 mm maximum. The device is priced at $1.25 per unit in 3,000 quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.