ON Semiconductor Expands PYTHON Family of CMOS Image Sensors with Compact, SVGA Offering

November 01, 2016

New 1/3.6-inch device brings industrial-level sensitivity and performance to cost-effective, small-footprint applications

PHOENIX, AZ – Nov. 1, 2016 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is bringing the advanced global shutter imaging performance of the PYTHON CMOS image sensor family to a cost-effective, small-footprint design.

The new PYTHON 480 image sensor shares the same pixel design and SVGA (800 x 600 pixel) resolution as the existing PYTHON 500, but is optimized for both size (with a package 85% smaller than the existing device) and power. Large 4.8 µm global shutter pixels with two available microlens offset options enable high light sensitivity in end-use cases ranging from inspection systems (where short exposure times enable the capture of moving objects without motion blur) to barcode scanning (where large depth of field and small scanning engines are needed). The new device preserves the imaging performance of the PYTHON family of CMOS image sensors while supporting readout speeds of up to 120 frames per second (fps) through either a single-lane LVDS or parallel output.

“The PYTHON family of CMOS image sensors has quickly become an industry standard for cost-effective, high-performance industrial imaging,” stated Herb Erhardt, Vice President and General Manager, Industrial Solutions Division, Image Sensor Group at ON Semiconductor. “With the PYTHON 480, the capabilities of this family are now available to a new tier of imaging applications that were formerly constrained by size, power and cost, providing them with the advanced imaging performance they require.”

The PYTHON 480 is sampling today in Monochrome and Bayer Color configurations in a RoHS-compliant CSP-67 package, with production planned for 1Q2017. A demonstration of the new PYTHON 480 as well as information on the full portfolio of PYTHON image sensors, including low-power, cost-effective configurations of the PYTHON 1300 and PYTHON 5000, will be available at ON Semiconductor’s booth (1C32) at the 2016 VISION trade fair, November 8 - 10 in Stuttgart, Germany.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.