Interfacing PN532 NFC with RSL10

Hello,

I wanted to know whether there is any way to interface the PN532 NFC module with RSL10.

@pallavi.arage

PN532 NFC module has I2C or SPI interface so it would be possible.

Based on the information on the module (V_cc= 5V) you need use voltage level translator. Our RSL10 EVB can’t support that.

RSL10 has CMSIS examples for I2C_cmsis_ driver as well as SPI_cmsis_driver.

In CMSIS configuration wizard you can configure I2C or SPI interface.

image

Thank you for using our community forum!