Solutions

Connectivity is what enables the “I” in the Internet-of-Things (IoT). From wired connectivity solutions, prevalent in industrial settings, to wireless solutions, popular in consumer areas, there are many options available to system architects. Attributes such as data rate, range, throughput, supported topologies, security, and energy efficiency all need to be taken into account

onsemi offers a wide range of ultra-low power, robust, best-in-class Rx sensitivity transceivers, and System-on-Chip (SoC) and System-in-Package (SiP) solutions to cater to various IoT applications. Our solutions span short range wireless technologies, including Bluetooth® Low Energy, Wi-Fi and the Green Power™ protocol, as well as longer-range technologies. With best-in-class energy efficiency, solutions from onsemi enable the creation of long battery life IoT devices. Fully certified stacks (ETSI, FCC, etc.) and development tools significantly reduce time-to-market in deploying IoT solutions.

Power Over Ethernet (PoE)
Bluetooth Low Energy
ZIGBEE
Wi-Fi

Interactive Block Diagram

2 Add a part
Select checkbox next to product and then Add to Worksheet button.
3 Download the worksheet
Worksheet Preview:
Application Block Product Taxonomy Part

Evaluation/Development Kits

RSL10 Smart Shot Camera

Connected Lighting Platform

Sensor Development Kits

Energy Harvesting Platforms

RSL10 Software Development Kit

Technical Documents

Wi−Fi Sensing: Revolutionizing Motion Sensing with Wi−Fi technology

While Wi−Fi is well known and universally used as a communication protocol, interest has grown recently in using the properties of the Wi−Fi signal itself to enable new applications.

Creating a State-of-the Art, Cost Effective Energy Harvesting Bluetooth Low Energy Switch

As IoT rapidly grows into new markets such as MHealth, Agriculture 4.0, and building automation, new questions are being raised about the energy required to support its growth.

Blyott Case Study:RSL10-based Beacon with Indoor Localization

Tatwah, an onsemi® technology partner, equipped Blyott with an onsemi Bluetooth Low Energy solution that provides extended battery life – the RSL10 System-in-Package (SiP)

Videos