SOLUTIONS
MADE
TOGETHER
Subaru & ON Semiconductor partner to drive innovation
Subaru and ON Semiconductor have partnered to revolutionize vehicle safety. Using our latest sensor technology, Subaru is developing life-saving systems like EyeSight® and DriverFocus™. With the right tools, Subaru is changing the rules of the road. So, what will we do together?
You Bring the Talent. We Bring the Tools.
Media
Resources
A Closer Look Into The Making of the Eyesight Driver Assist Platform by Subaru
What is particularly interesting about the EyeSight system is how closely Subaru and ON Semiconductor® worked together to develop the solution. This is unusual in a sector that is so vertically integrated. Hierarchically, it is arranged in tiers. Normally, an automotive manufacturer would work predominantly with Tier 1 suppliers who, in turn, work with Tier 2 suppliers and so on. ON Semiconductor supplies to Tier 1 and Tier 2 manufacturers.
Subaru Selects ON Semiconductor Image Sensing Technology for its New-Generation EyeSight® Driver Assist Platform
ON Semiconductor and SUBARU redefine leading-edge ADAS capability with new machine vision algorithms and sensing technology
ON Semiconductor's image sensors continue to provide the eyes for the new generation of Subaru's advanced EyeSight® driver assist system
This time last year, we published an update about how ON Semiconductor's CMOS sensors were enabling Subaru's EyeSight Driver Assist Technology, and now we're back to present the next chapter in this exciting area. EyeSight is an advanced driver assist system, or ADAS. By now, many drivers are familiar with the concept of ADAS, but it's worth noting that, just like vehicles, ADAS takes various forms, each with its own feature-set. The ADAS features offered by in vehicles from different manufacturers are likely to be similar, but the way they implement the ADAS varies. This variation really comes down to delivering the user experience that the OEM is aiming to provide.
ON Semiconductor Ships 100 Million Image Sensors for Camera-based ADAS Systems in Support of Customers like SUBARU
ON Semiconductor and SUBARU continue their collaboration on the EyeSight Driver Assistance System with a shared vision of improving road safety
ON Semiconductor ADAS Technology Enables ‘Eyes’ for SUBARU’s EyeSight Driver Assist Technology
A few years ago, you could have been forgiven for thinking that vehicles with the ability to ‘see’ the road ahead and assist the driver in critical conditions were nothing more than science fiction. However, recent and ongoing developments in automotive technology mean new vehicles are more likely to have some ability to detect their environment and take direct action contributing to improved road, passenger and pedestrian safety.
Design
Resources
CMOS Image Sensor, 2.3 MP, 1/2.7"
The AR0231AT is a 1/2.7-inch CMOS digital image sensor with an active-pixel array of 1928Hx1208V. It includes LED Flicker Mitigation (LFM) that eliminates high frequency LED flicker from traffic signs and vehicle LED lighting and allows Traffic Sign Reading algorithms to operate in all light conditions. The AR0231AT uses the latest 3.0 micron Back Side Illuminated (BSI) pixel with ON Semiconductor’s DR-Pix™ technology, which offers dual conversion gain for improved performance under all lighting conditions. It captures images in linear, HDR or LFM modes, and offers frame-to-frame context switching between modes. The AR0231AT also includes features that support ASIL B.
CMOS Image Sensor, 1.2 MP, 1/3", Global Shutter"
This 1/3-inch format, 1.2 MP imaging device has been designed to address the challenging requirements of automotive in-cabin cameras. The new global shutter sensor allows the camera to “freeze” fast moving scene data, and ensures effective synchronization with pulsed light sources. The AR0135 sensor incorporates a new innovative global shutter pixel design, with 10X lower dark current and 4X higher shutter efficiency vs. previous generation products. These improvements allow the sensor to produce clear, low-noise images, in both low-light and bright scenes, and in high temperature environments. This performance enables the required eye tracking and gesture detection functionality in next generation automotive in-cabin systems.
CMOS Image Sensor, 1.2 MP, 1/3"
ON Semiconductor's AR0132AT 1/3-inch CMOS digital image sensor with an active-pixel array of 1280H x 960V. It captures images in either linear or high dynamic range modes, with a rolling-shutter readout. It includes sophisticated camera functions such as auto exposure control, windowing, and both video and single frame modes. It is designed for both low light and high dynamic range scene performance. It is programmable through a simple two-wire serial interface. The AR0132AT produces extraordinarily clear, sharp digital pictures, and its ability to capture both continuous video and single frames makes it the perfect choice for a wide range of applications, including surveillance and HD video. This sensor is compatible with ON Semiconductor's automotive image co-processors which provides megapixel HDR image processing.
Chip Supply Voltage Monitor Limits
This application note provided details of how the chip supply voltage monitor limits were established for the AR0220AT, AR0231AT and AR0138AT. This document includes the suggested limits, and the analysis used to arrive at those limits.