feedback
Rate this webpage
Need
Support?

Selected Industrial Automation Solution
Selected Solution
Return to Industrial Automation solution

Industrial LiDAR

LiDAR sensing is a trending solution for Industrial Automation and Control Systems because it is cost-effective, highly accurate, fast, and scalable. LiDAR sensing using SiPM (Silicon Photomultiplier) arrays also enables object detection and avoidance as well as movement and occupancy detection.

ON Semiconductor SiPM arrays feature an innovative fast mode that decreases sensing time. Our SiPM technology has industry-leading efficiency and dynamic range, enabling the sensors to work in a wide variety of environments, including direct sunlight.

ON Semiconductor offers LiDAR solutions alongside a wide range of LiDAR development platforms and tools supported by highly technical and experienced applications engineers to assist product development.

Product Technologies
RB-Series
The RB-Series is a family of NIR-enhanced Silicon Photomultipliers (SiPM) for LiDAR and ranging applications using near-infrared illumination such as 905nm and 940nm.
RDM


RDM
The RDM SiPM 1x12 array is an automotive grade NIR-enhanced Silicon Photomultiplier (SiPM) array for LiDAR applications using near-infrared illumination such as 905nm and 940nm.
RB-Series


Evaluation/Development Tools
SiPM dToF LiDAR Platform
The Direct Time of Flight (dToF) SiPM LiDAR Platform is a single point range finder development kit for cost-optimized industrial and commercial applications.
SECO-RANGEFINDER-GEVK
ARRAYRDM-0112A20-GEVB
This product allows users to quickly and easily set up an evaluation of the ArrayRDM-0112A20-QFN 1x12 element silicon photomultiplier (SiPM) array.
ARRAYRDM-0112A20-GEVB
Technical Documents
A Brief Introduction to Silicon Photomultiplier (SiPM) Sensors
The Silicon Photomultiplier (SiPM) is a low-light sensor that has performance characteristics comparable to a conventional PMT with the practical advantages of a solid-state sensor. The SiPM is well suited to a variety of applications including LiDAR, medical imaging, radiation detection and biosciences.
A Brief Introduction to Silicon Photomultiplier (SiPM) Sensors
SiPMs in Direct ToF Ranging Applications
This white paper is intended to assist in the development of SiPM (Silicon Photomultiplier) based LiDAR (Light Detection and Ranging) systems. The following sections contain information on the design and implementation of a direct ToF (Time-of-Flight) rangefinder, in terms of the laser, timing and optical parameters and detailed analysis of key aspects that must be considered when integrating SiPMs in such systems.
SiPMs in Direct ToF Ranging Applications
Direct Time−of−Flight Depth Sensing Reference Designs
Depth sensing with precise measurements is a requirement for many applications in today’smarkets, including industrial, consumer, and automotive.
Direct Time−of−Flight Depth Sensing Reference Designs
Biasing and Readout of ON Semiconductor SiPM Sensors
The SiPM consists of an array of microcells. Each microcell consists of a Single Photon Avalanche Diode (SPAD) and a quench resistor. ON Semiconductor SiPMs have 3 terminals; cathode, anode and fast output.
Performance Measurement and Model Validation of the ON Semiconductor Gen3 Scanning LiDAR Demonstrator
These sensors are now at the forefront of the most innovative developments for LiDAR applications in ADAS (Advanced Driver Assistance Systems) and autonomous vehicles.
Direct Time-of-Flight Depth Sensing Reference Designs
This document provides an overview of various Time-of-Flight depth sensing reference designs.
Videos


Developing a Direct Time of Flight dToF LiDAR Range Finder

Introduction to Industrial Rangefinding and the SiPM dToF LiDAR Platform, by Oriol Fillo and Edel Cashman for Electronica 2020



What is Industrial Rangefinding?

Introduction to the SiPM dToF LiDAR Platform



SiPM dToF LiDAR Platform GUI Walkthrough

How to use the SiPM dToF LiDAR Platform



Which Wavelength Will Prevail for Automotive LiDAR The Great Debate

Which wavelength will prevail for Automotive LiDAR?



Gen3 SIPM LiDAR Demonstrator System Outdoor Testing

Here we show our Gen 3 Scanning LiDAR Demonstrator in a live outdoor test. The demonstrator has an 80 degree x 5 degree FoV, RA-Series 1 x 16 SiPM Arr...



Gen3 SiPM LiDAR Demonstrator System Indoor Testing

In this video we show a SensL 1x16 C-Series in an 80 x 5 degree coaxial scanning LiDAR demonstrator. Various use cases are shown with low and high refl...



SensL Solid State LiDAR Design Considerations

Learn how silicon photomultipliers (SiPM) can be used in solid state LiDAR for ADAS and autonomous vehicles. We explain core LiDAR concepts and show...



Wade Appelman Autosens Interview

Learn from Wade Appelman for how ON Semiconductor is preparing for Autosens.

Your request has been submitted for approval.
Please allow 2-5 business days for a response.
You will receive an email when your request is approved.
Request for this document already exists and is waiting for approval.