Selected Connectivity Solution
Selected Solution
Return to Connectivity solution
SIGFOX

Sigfox, a Low Power Wide Area (LPWA) protocol, enables the simplest and lowest cost connectivity option for IoT devices. Sigfox devices do not require any pairing operations and are ready to use right out of the box. Sigfox devices typically transmit infrequently and have very long battery lives with very long RF range.
With a solution for all global Sigfox regions, ON Semiconductor is a market leader in Sigfox devices with strong relationships with strategic customers and partners.
We offer certified AT and API versions of worldwide Sigfox System-on-Chip (SoC) and System-in-Package (SiP) solutions to ease design-in and speed up deployment.
Products
AX-SFAZ: RF Transceiver SoC, Sigfox Verified RCZ4, Ultra-low Power
The AX-SFAZ is a single chip solution for a node on the Sigfox network in RCZ4 region. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE. This void is now filled by Sigfox, the ultra low power cellular connectivity solution.

AX-SFAZ-API: RF Transceiver SoC, Sigfox Verified RCZ4, Ultra-low Power, with API library
The AX-SFAZ-API is a single chip solution for a node on the Sigfox network. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE.

AX-SFEU: RF Transceiver SoC, Sigfox Verified RCZ1, Ultra-low Power’
The AX-SFEU is a single chip solution for a node on the Sigfox network. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE. This void is now filled by Sigfox, the ultra low power cellular connectivity solution.

AX-SFEU-API: RF Transceiver SoC, Sigfox Verified RCZ1, Ultra-low Power’ with API Library.
The AX-SFEU-API is a single chip solution for a node on the Sigfox network. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE.

AX-SFJK: RF Transceiver SoC, Sigfox Verified RCZ3&7, Ultra-low Power
The AX-SFJK is a single chip solution for a node on the Sigfox network in RCZ3 region. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE. This void is now filled by Sigfox, the ultra low power cellular connectivity solution.

AX-SFJK-API: RF Transceiver SoC, Sigfox Verified RCZ3&7, Ultra-low Power, with API library.
The AX-SFJK-API is a single chip solution for a node on the Sigfox network. In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE.

AX-SFUS: RF Transceiver SoC, Sigfox Verified RCZ2, Ultra-low Power’
The AX-SFUS is a single chip solution for a node on the Sigfox network in RCZ2 region (Americas) . In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE. This void is now filled by Sigfox, the ultra low power cellular connectivity solution.

AX-SFUS-API: RF Transceiver SoC, Sigfox Verified RCZ2, Ultra-low Power, with API Library
The AX-SFUS is a single chip solution for a node on the Sigfox network in RCZ2 region (Americas) . In the Internet of Things the domain of nation wide coverage and ultra low power consumption for smallest amounts of data can not be addressed by established standards such as GPRS or LTE. This void is now filled by Sigfox, the ultra low power cellular connectivity solution.

AX-SIP-SFEU: RF Transceiver System In Package, Sigfox Verified RC1, Ultra-low Power
AX−SIP−SFEU is an ultra−low power, ultra compact System-in-Package (SiP) solutions for a node on the Sigfox network with both up− and down−link functionality. Delivered with conformal shielding, the AX−SIP−SFEU SiP, contains all the necessary components and firmware for transmit and receive operation on the RC1 Sigfox network

AX-SIP-SFEU-API: RF Transceiver System In Package, Sigfox Verified RC1, Ultra-low Power
AX−SIP−SFEU is an ultra−low power, ultra compact System-in-Package (SiP) solutions for a node on the Sigfox network with both up− and down−link functionality. Delivered with conformal shielding, the AX−SIP−SFEU SiP, contains all the necessary components and firmware for transmit and receive operation on the RC1 Sigfox network.

Evaluation Boards
EU-SIGFOX-GEVB: IoT IDK EU SigFox Evaluation Board
The SIGFOX shield evaluation board demonstrates the AX-SFEU, a single chip solution to create an ultra low power consumption node on the Sigfox network for RCZ1 region (Europe), Internet of Things applications.

US-SIGFOX-GEVB: IoT IDK US SigFox Evaluation Board
The SIGFOX shield evaluation board demonstrates the AX-SFUS, a single chip solution to create an ultra low power consumption node on the Sigfox network for RCZ2 region (Americas), Internet of Things applications.

DVK-SFAZ-1-GEVK: Sigfox AT Development Kit for RCZ4
The miniature (13mm x 48mm) Sigfox development kit (DVK), DVK-SFAZ-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ4 region using the AX-SFAZ solution.

DVK-SFEU-1-GEVK: Sigfox AT Development Kit for RCZ1
The miniature (15mm x 33mm) Sigfox development kit (DVK), DVK-SFEU-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ1 region using the AX-SFEU solution.

DVK-SFUS-1-GEVK: Sigfox AT Development Kit for RCZ2
The miniature (13mm x 44mm) Sigfox development kit (DVK), DVK-SFUS-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ2 region using the AX-SFUS solution.

DVK-SFJK-1-GEVK: Sigfox AT Development Kit for RCZ3
The miniature (13mm x 35mm) Sigfox development kit (DVK), DVK-SFJK-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ3 region using the AX-SFJK solution.

DVK-SFAZ-API-1-GEVK: Sigfox API Development Kit for RCZ4
The miniature (13mm x 48mm) Sigfox development kit (DVK), DVK-SFAZ-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ4 region using the AX-SFAZ-API SoC solution.

DVK-SFEU-API-1-GEVK: Sigfox API Development Kit for RCZ1
The miniature (15mm x 33mm) Sigfox development kit (DVK), DVK-SFEU-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ1 region using the AX-SFEU-API SoC solution.

DVK-SFUS-API-1-GEVK: Sigfox™ API Development Kit for RCZ2
The miniature (13mm x 44mm) Sigfox development kit (DVK), DVK-SFUS-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ2 region using the AX-SFUS-API SoC solution.

DVK-SFJK-API-1-GEVK: Sigfox™ API Development Kit for RCZ3
The miniature (13mm x 35mm) Sigfox development kit (DVK), DVK-SFJK-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ3 region using the AX-SFJK-API SoC solution.

DVK-SIP-SFEU-1-GEVK: SIP SFEU DVK
The miniature (15mm x 27mm) Sigfox development kit (DVK), DVK-SIP-SFEU-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ1 region using the AX-SIP-SFEU solution.

DVK-SIP-SFEU-API-1-GEVK: SIP SFEU API DVK
The miniature (15mm x 27mm) Sigfox development kit (DVK), DVK-SIP-SFEU-API-1-GEVK, allows designers to quickly develop Sigfox connected applications in the RCZ1 region using the AX-SIP-SFEU-API SoC solution.