Which example is best to start to develop my application?

Hello,
My RSL10 application need below functions,
peripheral server with bonding(passkey), gatt custom service, UART, ADC, deep sleep, flash read/write for application data.
Which example is best for it?

Thanks,
Calvin

@Calvin

Please refer to the following pack examples:

  1. Here is link for passkey application.
    KB: How to support BLE passkey paring mode
  2. Gatt custom service, UART — peripheral_server_uart
  3. Deep sleep — sleep_ram_retention
  4. flash read/write — I think they might ask NVR1/2 read/write – ble_peripheral_server_bond.

We don’t have an example which covers all of them at this moment.

Thank you for using community forum.

2 Likes

It helped a lot.
Thank you.

5 Likes