Hey everyone
I try to build an ML algorithm with SensiML. Therefore I do the Slide Demo Project as stated by sensiml. The data collection with RSL10-SENSE-GEVK and RSL10-SIP-001-GEVB worked fine. Also the labeling and training of the algorithm. The test when the model runs on data capture lab with data streaming from RSL10-SENSE-GEVK worked as well. But if the model is run on the RSL10-SENSE-GEVK the model outputs the false state of the system. As stated in the sensiml software getting started guide I replaced the files in the sensiml folder and KNOWLEDGE_PACK is defined.
Has someone an idea wehre the error could be? It is most likley somthing with the integration of the model on the rsl10 because the model works outside of the rsl10.
Thank you for the help.
Kind Regards
Mischa
Some Information about my packs:
ONSemiconductor.BDK v. 1.19.0
ONSemiconductor.RSL10 v. 3.6.465
ONSemiconductor.RSL10SensiML v. 1.0.1
ARM.CMSIS v. 5.8.0
ARM.CMSIS-FreeRTOS v. 10.4.6
onsemi IDE Version: 4.1.2.79 running on windows 10