RSL10 SIP Package Drawings question

Hi Sir

Please kindly provide the following information.

  1. What is the Y-axis distance at the red box in the figure below?
  2. The relative position information of keepout and any pin?

  1. What is the Y-axis distance at the red box in the figure below?

0.300

  1. The relative position information of keepout and any pin?

I don’t understand quite what you’re asking. The cad files with dimensions can be found here: RSL10 SiP CAD Drawings

1 Like

Hi Jamie
Regarding question 2. that I think the file of the RSL10 SiP CAD drawing should solve my problem.
Many thanks.

5 Likes

Please kindly help to answer the following questions.

  1. Is the red keepout drawn along the red arrow in the figure below (to be aligned with the land)?
    image

  2. Is the green keepout drawn along the two red lines in the figure below?

  3. Is the green keepout drawn on the center of the land (at the red arrow in the figure below)?
    image

Yes to all three questions.

Thank you for using the Community Forum.