RSL10 sample FW for OTA test

Hi,

I built a custom board with integrated antenna.
I would like to evaluate the antenna performance in the anechoic chamber.
The test setup is based on the Rohde Schwarz CMW270 that needs to setup a connection with the DUT.
Is there a sample FW I can use?

Thanks

Hi @Alberto,

We have available hci_app firmware in CMSIS pack, which is intended to use with BLE certification and testing by enabling continuous wave broadcasting. It can be used to test the BLE capabilities. This firmware could be probably used also for OTA test and to determine the antenna performance.

Thank you for using our Community Forum.