Map file shows *IRQHandler's have same address?

My map file shows the following:

 .text          0x00135578       0x14 C:/Repos/../fota/build\libfota.a(fota_startup.S.o)
                0x00135578                NMI_Handler
                0x0013557a                HardFault_Handler
                0x0013557c                MemManage_Handler
                0x0013557e                BusFault_Handler
                0x00135580                UsageFault_Handler
                0x00135582                SVC_Handler
                0x00135584                DebugMon_Handler
                0x00135586                PendSV_Handler
                0x00135588                SysTick_Handler
                0x0013558a                UART_ERROR_IRQHandler
                0x0013558a                DSP7_IRQHandler
                0x0013558a                BLE_COEX_RX_TX_IRQHandler
                0x0013558a                DSP2_IRQHandler
                0x0013558a                MEMORY_ERROR_IRQHandler
                0x0013558a                WATCHDOG_IRQHandler
                0x0013558a                DIO1_IRQHandler
                0x0013558a                DIO3_IRQHandler
                0x0013558a                DSP3_IRQHandler
                0x0013558a                RF_TXFIFO_IRQHandler
                0x0013558a                RTC_ALARM_IRQHandler
                0x0013558a                SPI0_ERROR_IRQHandler
                0x0013558a                BLE_COEX_IN_PROCESS_IRQHandler
                0x0013558a                DIO0_IRQHandler
                0x0013558a                DMA5_IRQHandler
                0x0013558a                ASRC_IN_IRQHandler
                0x0013558a                SPI1_ERROR_IRQHandler
                0x0013558a                DMIC_OD_ERROR_IRQHandler
                0x0013558a                PCM_TX_IRQHandler
                0x0013558a                SPI0_TX_IRQHandler
                0x0013558a                UART_TX_IRQHandler
                0x0013558a                Default_Handler
                0x0013558a                DMIC_OUT_OD_IN_IRQHandler
                0x0013558a                ADC_BATMON_IRQHandler
                0x0013558a                DMA7_IRQHandler
                0x0013558a                PCM_RX_IRQHandler
                0x0013558a                RF_TX_IRQHandler
                0x0013558a                SPI0_RX_IRQHandler
                0x0013558a                ASRC_ERROR_IRQHandler
                0x0013558a                RF_RXSTOP_IRQHandler
                0x0013558a                DSP1_IRQHandler
                0x0013558a                WAKEUP_IRQHandler
                0x0013558a                RF_SYNC_IRQHandler
                0x0013558a                SPI1_RX_IRQHandler
                0x0013558a                CLKDET_IRQHandler
                0x0013558a                DSP6_IRQHandler
                0x0013558a                TIMER2_IRQHandler
                0x0013558a                AUDIOSINK_PERIOD_IRQHandler
                0x0013558a                TIMER0_IRQHandler
                0x0013558a                DMA3_IRQHandler
                0x0013558a                RTC_CLOCK_IRQHandler
                0x0013558a                DIO2_IRQHandler
                0x0013558a                DMA0_IRQHandler
                0x0013558a                ASRC_OUT_IRQHandler
                0x0013558a                PCM_ERROR_IRQHandler
                0x0013558a                DSP5_IRQHandler
                0x0013558a                DMA4_IRQHandler
                0x0013558a                UART_RX_IRQHandler
                0x0013558a                FLASH_ECC_IRQHandler
                0x0013558a                SPI1_TX_IRQHandler
                0x0013558a                RF_IRQ_RECEIVED_IRQHandler
                0x0013558a                DSP4_IRQHandler
                0x0013558a                DMA6_IRQHandler
                0x0013558a                RF_RXFIFO_IRQHandler
                0x0013558a                DMA1_IRQHandler

Why IRQHandlers from UART* to the end share the same address 0x0013558a?
Do I interpret this map file incorrectly?

I believe that means the code doesn’t implement any of those handlers and they all go to a default handler.