Hi,
Sorry of this is the wrong category but couldn’t find the right one (only had available site feedback or connectivity). I am looking for a low power, 3V sensorless brushless dc motor controller and came across the LV8806. I have two questions:
- In regards to the direction control pin, can this be changed dynamically or must it be fixed at start up and remain fixed?
- In the case of a Beat Lock as described in the application note, is this condition reported by the RD pin as motor locked?
- Are there any specs in regards to the minimum BEMF constant that the motor should have to work with this IC?
Thanks