Ke_get_max_mem_usage API Undefined

Hi,

I am running ble_peripheral_server_bond code on RSL10. I want to read the memory usage. I am trying to use API ke_get_max_mem_usage to read heap size in use. I have enabled CFG_DBG macro which sets KE_PROFILING to 1. But when I added this in app.c gives undefined function error. I have added header ke_mem.h and ke_config.h in app.c.

Can you help me on this

Thanks
Kavya

@kavya.ms

This API (function) is not available for full BLE stack. That is only available for HCI and MFi.
What is the purpose that you would like to use this?
When you call ke_malloc(), if there is no space, application will reset.