KB: Procedure for Reading & Writing to RSL10 Flash Memory


[RSL10 - Knowledge Base]


Question

The RSL10 includes 384 KB of flash memory, allowing users to take advantage of its non-volatile features. The flash memory is used for storing user application and data, Bluetooth stack software, Bluetooth profiles, and the LPDSP32 application firmware. The flash memory is organized into sectors, each containing 2048 bytes of flash memory.

What is the procedure to safely and effectively write to and read from this flash memory?


Recommendation

Section 7.3 of the RSL10 Hardware Reference, “Flash Memory Operations”, provides a step-by-step execution guide of how the Read & Write operations can be completed safely while ensuring the integrity of the memory contents. The RSL10 Hardware Reference is available in our RSL10 Documentation Package, but is also included installations of the RSL10 Software CMSIS Pack.


1 Like