KB: Getting setup with RSL10 using IAR & Keil

Question

What steps are necessary to program the RSL10 from Keil or IAR tools?

Recommendation

  1. Go to the RSL10 product page page
  2. Download the RSL10 Getting Started Guide and the RSL10 Software Package by clicking the associated download buttons on the site (see image below). Within that manual are dedicated chapters for setting up IAR & Keil environments for use with the RSL10 CMSIS-Pack, which is part of the RSL10 Software Package.
  3. Also within the RSL10 Software Package is a set of sample projects. Those that are compatible with IAR & Keil are listed in the RSL10 Sample Code User’s Guide.

Note: for those who would rather use the Eclipse IDE, follow the instructions on this page.