Question
What steps are necessary to access the RSL10 SDK and set up the Eclipse based tools
Recommendation
- Go to the RSL10 product page page
- Use the download buttons on the main page
- Download and read the
RSL10 Getting Started Guide
for detailed instructions - Download and install the Eclipse based
ON Semiconductor IDE Installer
- Download and unzip the
RSL10 Software Package
which contains the RSL10 CMSIS Pack - Follow instructions in the
RSL10 Getting Started Guide
to install the CMSIS Pack and sample projects - Other optional downloads are available, such as the
RSL10 Bluetooth Mesh Package
, theRSL10 USB Dongle BLE Explorer
, theRSL10 Software Utility Apps
, and theRSL0 LPDSP Software Package
.
Note 1: The RSL10 Documentation Package
is provided as a separate download in the list, and its contents are also included in the RSL10 Software Package
so it does not need to be downloaded if the software package is installed.
Note 2: The RSL10 Software Package
also includes the release notes document
Note 3: MyON accounts are required to download many of these packages. An account can be created here
Note 3: The CMSIS pack is also compatible with IAR & Keil. More details are available here.
Note 4: Setting up the tools to program the LPDSP32 is a separate process described in this post.