KB: Expected Flash Memory Endurance

Question

What are the flash memory endurance specifications for RSL10?

Answer

As per the RSL10 datasheet, below are the access cycles and longevity expectations.

Note: A description of the flash memory mapping, including the Non-Volatile Record (NVR) Sectors, is included in the Memory chapter of the Hardware Reference Manual as part of the RSL10 Documentation Package.