Question
The DIO status is at 200 us – high level voltage – when RSL10 wakes up. We need to configure the DIO pin to stay at low voltage after RSL10 wakes up. How do we do this?
The DIO status is at 200 us – high level voltage – when RSL10 wakes up. We need to configure the DIO pin to stay at low voltage after RSL10 wakes up. How do we do this?
You can reconfigure that DIO in system_rsl10.c.
Use this for DIO configuration:
Sys_DIO_Config(DIO number,DIO_MODE_GPIO_OUT_0|DIO_NO_PULL|DIO_LPF_DISABLE);
Using this, I have not seen a high pulse in the running period.