IDE Upgrade Issues

Hi,

I used the onsemi example project to find the issue and read through the posts. We tried the following approach, which didn’t solve the issue.

I can debug the normal hrp_fota example but not the hrp_fota_sleep.

I attached the two error messages I get.

Are there settings I have to do in addition, so the sleep example can be debugged?

thanks,
see attached:


Hello Youssef,
Did you upload bootloader first ?
Also which debugger do you use ?

I uploaded the bootloader first through the Stand Alone Flashloader as well as the IDE before flashing the sleep example. It made no difference.

I have tried this with the onsemi RSL10 Eval Board as well as the Segger Edu mini and our own hardware. Both show the same error.

@youssef.bouguerba

Please try to implement suggestions from our RSL10 Getting Started Guide, Chapter 7.4 7.4 DEBUGGING WITH LOW POWER SLEEP MODE .