I am trying to get familiar with the dev board and have not been able to program the device. I have only the board and my laptop and get the feeling I need additional hardware, perhaps a j-link programmer? Can somebody explain what else I need and/or how to connect the pieces so I can program the device?
I can build the smartshot_demo_cam project in the IDE but have been hesitant to do the debugging step as I only have a single dev board and don’t want to break it. I also tried to run jlink.exe manually and it doesn’t see the board.
Hello @miked531
The SECO-RSL10-CAM-GEVB board does not contain an On-Board Debugger.
You need to use an external J-Link debug probe to flash/debug the device.
Additionally you need an 9-Pin Cortex-M Adapter (sometimes also listed as 10-pin) to connect the probe to the board.
The USB port can be used to update the Image Sensor Processor only, but this step should not be required.
Best regards,
Lukas
Can you suggest which devices specifically, that I need? Links and/or model numbers would be extra helpful.
Looks like about the only place to connect a 9-pin adapter is to CON2, correct?
Any of the currently available J-Link debug probes will work with RSL10.
https://www.segger.com/products/debug-probes/j-link/
https://www.segger.com/products/debug-probes/j-link/accessories/adapters/9-pin-cortex-m-adapter/
For debugging you power the board via USB cable and connect the 9-pin adapter cable from J-Link to CON2.
After that you can launch debugging session from the IDE.
Best regards,
Lukas