High-side Power path controller

Hello,

I was wondering if you have any similar alternatives to LTC LTC4416EMS#PBF or Maxim MAX5944ESE+?
The two input voltages are 19V@10A cont. max and 5V@15A and the two rails would be controlled (ON/OFF) by the user via a low-voltage 3-state switch.

By the way, why are there no power management-related category to choose from?

Thanks & regards,

Al

Hi,

As this Community Forum is intended to discuss connectivity products and solutions from ON Semiconductor for Bluetooth Low Energy, Zigbee and Sub-GHz, we would like you to redirect your question to our technical support team at technical support which provides up to date information and services to meet your needs.

Thank you.