Flash_WriteBuffer Max Number of Words?

What is the maximum number of words that accepts Flash_WriteBuffer?

The maximum number of words is 2^32 - 2.

@jamie.meacham Recently, I noticed that the hardware reference has been updated with SDK 3.5. In the Release Notes it is mentioned that “Hardware Reference: Flash_WriteBuffer() has a
maximum length of 32 words”. This is a bit confusing; is the maximum length of the buffer argument 64 words (i.e. 256 bytes)?

Please disregard that update. The note stating a limit of 32 words is in error and is being removed in future releases.

Thank you for using the Community Forum.

2 Likes

Thank you for the clarification.

4 Likes