Flash memory usage for Application Data

Hi,
We are currently using RSL10 for our application development.
For the application I am required to store 65KB of data.

From the “RSL10 Firmware Over-The-Air User’s Guide” Section 3.1
“The Bluetooth Low Energy stack, which contains the Device Firmware Update (DFU) component and the padding between the sub-images, allocates about 154KB. The remainder of the RSL10 main flash memory is available for the application (380KB - 154KB - 8KB approximately equal to 218KB).”

Is this true in case of RTOS built image also?

Thanks & Regards,
Prasanna

@Prasanna

Please confirm these questions.

  1. Will this 65KB data save to RAM or need save to Flash?
  2. If it is in RAM, it might be able to use DSP_DRAM.
    If it is in Flash and it needs use FOTA, the calculation (380KB - 154KB - 8KB =218KB
    This is true. If it needs 65KB for store data, then only (218-65) KB for application.

You have asked similar question at " Flash writing to NVR and Flash Areas error".
We have provided reference code in there.

Thank you for using our community forum!

HI Martin,
I will be need to save the data in flash.

But I got the answer from the other question.

Thanks for your help

Best Regards,
Prasanna

3 Likes