Having trouble downloading code to the AXM0F243. This is NOT an eval board. When I download via AXcode:Blocks, I get the following:
Setting remote timeout to unlimited
Connecting to remote target
Setting breakpoints
Debugger name and version: GNU gdb (GNU Tools for ARM Embedded Processors) 7.10.1.20160923-cvs
Connected
In __Vectors () ()
However I’m not able to do any break points, that is the code will not break, can’t do a hardware or software reset, it just gives me the above message. Other times I will get the “No Devices Found” message when I try to download. It’s my understanding that I basically need VDD (which I have) and a 32768 clock to get a successful download and really disregarding everything else for now.
Any tips or advice??
Thank you!
Jon