Q: I noticed some AX5043 related part numbers are listed as last time buy or last shipments. Are you going to End of Life the AX5043?
A: NO! We ship millions of AX5043 every quarter, we have no short term plans to end of life this awesome product. What we did was get rid of the 500 piece reels, those are the only part numbers being discontinued. For example the AX5043-1-TA05 was a 500 part reel, and will no longer be supported. BUT the AX5043-1-TW30, which is a 3k reel, is fully supported.
Our distribution partners have smaller quantities available, so don’t worry about the lack of 500 unit reels.