Ezairo 7160 DIO connection for using the "ble_android_asha" in the built in RSl10

In the “ble_android_asha” sample program’s readme file, it says the following regarding the DIO connections:

But in the Ezairo 7100 firmware source code, the DIO pins are defined as follows

20210730_01_DIO_ezairo7110

The 7160 datasheet also shows that Ezairo DIO16 is connected to RSL10 DIO13
20210730_03_DIO_datasheet

Is this an error in the 7100 firmware source code? Should DIO_RX_IRQ be 15 or 16?

1 Like

Hi @mahaju

Please note that Ezairo products require NDA, therefore we would like you to redirect your question to our technical support team at technical support which provides up to date information and services to meet your needs.

Thank you.