I would like to encrypt data before storing it to an external memory connected to the RSL10. The basic encryption supported by the RSL10 seems to be AES ECB (accessed via BB_AESCNTL). The BLE communication uses AES CCM (shown in the baseband controller).
Is there a way to access the AES CCM to encrypt data outside of the BLE communication context (i.e. encrypt data to write to external memory)?
No. You can’t use the AES CCM. This is for BB only.
Please refer to RSL10 AES128 sample project, if you need to use AES.
You can use this block for hardware encryption and not for hardware decryption. You can only do software decryption.
Thank you for using our community forum!