Cannot keep connection in the deep sleep mode?

Hello,
After connected, it will be disconnected if entering to the deep sleep mode (wake up from flash).
Is it right? Is there any way to keep connection during the deep sleep mode (wake up from flash) ?

Thanks,
Calvin

@Calvin

Q1: After connected, it will be disconnected if entering to the deep sleep mode (wake up from flash).
Is it right?

A1: It is correct. sleep wakeup from flash is similar like power up.

Q2: Is there any way to keep connection during the deep sleep mode (wake up from flash) ?

A2: No. if you need keep connection , you need reference our peripheral_server_sleep (wakeup from RAM).

Please refer to our community forum thread: BLE sleep mode and deep sleep mode difference..

Thank you for using our community forum.

1 Like