Can I cancel "Generic Attribute Service"

Hi,

I’m developing a BLE application on the RSL10. I’m using with 3.2.608 SDK version.
I have tested the peripheral_server_sleep sample application on the RSL10 evaluation board 。

Please refer to the red box in the figure below,
Is it possible to remove the “0x1801” service?

Thanks.

image

@march0303.yao

Is it possible to remove the “0x1801” service?

Stack does not offer the ability to remove Generic Attribute Service.

The Generic Attribute Profile (GATT) establishes how data will be organized and exchanged over a Bluetooth® Low Energy (BLE) connection.

The Generic Attribute Profile (GATT) profile, defines the way that two Bluetooth® Low Energy (BLE) devices transfer data back and forth using concepts called Services and Characteristics
In this example peripheral_server_sleep :

Standard battery service : 180F

image

and

custom service

image

/* Custom service UUIDs */
#define CS_SVC_UUID                     { 0x24, 0xdc, 0x0e, 0x6e, 0x01, 0x40, \
                                          0xca, 0x9e, 0xe5, 0xa9, 0xa3, 0x00, \
                                          0xb5, 0xf3, 0x93, 0xe0 }

[/quote]

Thank you using our community forum !

Thank you martin.bela for your explanations

Best regards,

2 Likes